ACTION#.SOURCEPARAM

Description

ACTION#.SOURCEPARAM is used to configure an action source. Most sources do not require this parameter. For those sources, ACTION#.SOURCEPARAM is marked NotInUse.

For sources that do require this parameter, ACTION#.SOURCE must be set before ACTION#.SOURCEPARAM. When ACTION#.SOURCE is set, the units, range, and default value of ACTION#.SOURCEPARAM are updated, and the parameter is set to its default value.

Example

This example sets up a move complete action source for motion task 7 on axis 2.

>> ACTION1.SOURCE = 10 (Move complete)
>> ACTION1.SOURCEID = 2 (Axis 2)
>> ACTION1.SOURCEPARAM = 7 (Motion task 7)

Versions

Action Version Notes
Implemented 02-01-02-000

 

General Information

Type

Read/Write

Description Action source configuration parameter

Units

Depends on ACTION#.SOURCE

Range

Depends on ACTION#.SOURCE

Default Value

Depends on ACTION#.SOURCE

Data Type

Float

See Also ACTION#.SOURCE, ACTION#.SOURCEID

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.SOURCEPARAM

3906h

01h

Signed32

-

1000:1

Read/Write

No

ACTION2.SOURCEPARAM

3906h

02h

Signed32

-

1000:1

Read/Write

No

ACTION3.SOURCEPARAM

3906h

03h

Signed32

-

1000:1

Read/Write

No

ACTION4.SOURCEPARAM

3906h

04h

Signed32

-

1000:1

Read/Write

No

ACTION5.SOURCEPARAM

3906h

05h

Signed32

-

1000:1

Read/Write

No

ACTION6.SOURCEPARAM

3906h

06h

Signed32

-

1000:1

Read/Write

No

ACTION7.SOURCEPARAM

3906h

07h

Signed32

-

1000:1

Read/Write

No

ACTION8.SOURCEPARAM

3906h

08h

Signed32

-

1000:1

Read/Write

No

ACTION9.SOURCEPARAM

3906h

09h

Signed32

-

1000:1

Read/Write

No

ACTION10.SOURCEPARAM

3906h

0ah

Signed32

-

1000:1

Read/Write

No

ACTION11.SOURCEPARAM

3906h

0bh

Signed32

-

1000:1

Read/Write

No

ACTION12.SOURCEPARAM

3906h

0ch

Signed32

-

1000:1

Read/Write

No

ACTION13.SOURCEPARAM

3906h

0dh

Signed32

-

1000:1

Read/Write

No

ACTION14.SOURCEPARAM

3906h

0eh

Signed32

-

1000:1

Read/Write

No

ACTION15.SOURCEPARAM

3906h

0fh

Signed32

-

1000:1

Read/Write

No

ACTION16.SOURCEPARAM

3906h

10h

Signed32

-

1000:1

Read/Write

No

ACTION17.SOURCEPARAM

3906h

11h

Signed32

-

1000:1

Read/Write

No

ACTION18.SOURCEPARAM

3906h

12h

Signed32

-

1000:1

Read/Write

No

ACTION19.SOURCEPARAM

3906h

13h

Signed32

-

1000:1

Read/Write

No

ACTION20.SOURCEPARAM

3906h

14h

Signed32

-

1000:1

Read/Write

No

ACTION21.SOURCEPARAM

3906h

15h

Signed32

-

1000:1

Read/Write

No

ACTION22.SOURCEPARAM

3906h

16h

Signed32

-

1000:1

Read/Write

No

ACTION23.SOURCEPARAM

3906h

17h

Signed32

-

1000:1

Read/Write

No

ACTION24.SOURCEPARAM

3906h

18h

Signed32

-

1000:1

Read/Write

No

ACTION25.SOURCEPARAM

3906h

19h

Signed32

-

1000:1

Read/Write

No

ACTION26.SOURCEPARAM

3906h

1ah

Signed32

-

1000:1

Read/Write

No

ACTION27.SOURCEPARAM

3906h

1bh

Signed32

-

1000:1

Read/Write

No

ACTION28.SOURCEPARAM

3906h

1ch

Signed32

-

1000:1

Read/Write

No

ACTION29.SOURCEPARAM

3906h

1dh

Signed32

-

1000:1

Read/Write

No

ACTION30.SOURCEPARAM

3906h

1eh

Signed32

-

1000:1

Read/Write

No

ACTION31.SOURCEPARAM

3906h

1fh

Signed32

-

1000:1

Read/Write

No

ACTION32.SOURCEPARAM

3906h

20h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40700

1

40700 (0x9efc)

ACTION1.SOURCEPARAM

Signed32

Read/Write

Yes

40701

1

40701 (0x9efd)

ACTION2.SOURCEPARAM

Signed32

Read/Write

Yes

40702

1

40702 (0x9efe)

ACTION3.SOURCEPARAM

Signed32

Read/Write

Yes

40703

1

40703 (0x9eff)

ACTION4.SOURCEPARAM

Signed32

Read/Write

Yes

40704

1

40704 (0x9f00)

ACTION5.SOURCEPARAM

Signed32

Read/Write

Yes

40705

1

40705 (0x9f01)

ACTION6.SOURCEPARAM

Signed32

Read/Write

Yes

40706

1

40706 (0x9f02)

ACTION7.SOURCEPARAM

Signed32

Read/Write

Yes

40707

1

40707 (0x9f03)

ACTION8.SOURCEPARAM

Signed32

Read/Write

Yes

40708

1

40708 (0x9f04)

ACTION9.SOURCEPARAM

Signed32

Read/Write

Yes

40709

1

40709 (0x9f05)

ACTION10.SOURCEPARAM

Signed32

Read/Write

Yes

40710

1

40710 (0x9f06)

ACTION11.SOURCEPARAM

Signed32

Read/Write

Yes

40711

1

40711 (0x9f07)

ACTION12.SOURCEPARAM

Signed32

Read/Write

Yes

40712

1

40712 (0x9f08)

ACTION13.SOURCEPARAM

Signed32

Read/Write

Yes

40713

1

40713 (0x9f09)

ACTION14.SOURCEPARAM

Signed32

Read/Write

Yes

40714

1

40714 (0x9f0a)

ACTION15.SOURCEPARAM

Signed32

Read/Write

Yes

40715

1

40715 (0x9f0b)

ACTION16.SOURCEPARAM

Signed32

Read/Write

Yes

40716

1

40716 (0x9f0c)

ACTION17.SOURCEPARAM

Signed32

Read/Write

Yes

40717

1

40717 (0x9f0d)

ACTION18.SOURCEPARAM

Signed32

Read/Write

Yes

40718

1

40718 (0x9f0e)

ACTION19.SOURCEPARAM

Signed32

Read/Write

Yes

40719

1

40719 (0x9f0f)

ACTION20.SOURCEPARAM

Signed32

Read/Write

Yes

40720

1

40720 (0x9f10)

ACTION21.SOURCEPARAM

Signed32

Read/Write

Yes

40721

1

40721 (0x9f11)

ACTION22.SOURCEPARAM

Signed32

Read/Write

Yes

40722

1

40722 (0x9f12)

ACTION23.SOURCEPARAM

Signed32

Read/Write

Yes

40723

1

40723 (0x9f13)

ACTION24.SOURCEPARAM

Signed32

Read/Write

Yes

40724

1

40724 (0x9f14)

ACTION25.SOURCEPARAM

Signed32

Read/Write

Yes

40725

1

40725 (0x9f15)

ACTION26.SOURCEPARAM

Signed32

Read/Write

Yes

40726

1

40726 (0x9f16)

ACTION27.SOURCEPARAM

Signed32

Read/Write

Yes

40727

1

40727 (0x9f17)

ACTION28.SOURCEPARAM

Signed32

Read/Write

Yes

40728

1

40728 (0x9f18)

ACTION29.SOURCEPARAM

Signed32

Read/Write

Yes

40729

1

40729 (0x9f19)

ACTION30.SOURCEPARAM

Signed32

Read/Write

Yes

40730

1

40730 (0x9f1a)

ACTION31.SOURCEPARAM

Signed32

Read/Write

Yes

40731

1

40731 (0x9f1b)

ACTION32.SOURCEPARAM

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.SOURCEPARAM

40700

Float

Read/Write

-

ACTION2.SOURCEPARAM

40701

Float

Read/Write

-

ACTION3.SOURCEPARAM

40702

Float

Read/Write

-

ACTION4.SOURCEPARAM

40703

Float

Read/Write

-

ACTION5.SOURCEPARAM

40704

Float

Read/Write

-

ACTION6.SOURCEPARAM

40705

Float

Read/Write

-

ACTION7.SOURCEPARAM

40706

Float

Read/Write

-

ACTION8.SOURCEPARAM

40707

Float

Read/Write

-

ACTION9.SOURCEPARAM

40708

Float

Read/Write

-

ACTION10.SOURCEPARAM

40709

Float

Read/Write

-

ACTION11.SOURCEPARAM

40710

Float

Read/Write

-

ACTION12.SOURCEPARAM

40711

Float

Read/Write

-

ACTION13.SOURCEPARAM

40712

Float

Read/Write

-

ACTION14.SOURCEPARAM

40713

Float

Read/Write

-

ACTION15.SOURCEPARAM

40714

Float

Read/Write

-

ACTION16.SOURCEPARAM

40715

Float

Read/Write

-

ACTION17.SOURCEPARAM

40716

Float

Read/Write

-

ACTION18.SOURCEPARAM

40717

Float

Read/Write

-

ACTION19.SOURCEPARAM

40718

Float

Read/Write

-

ACTION20.SOURCEPARAM

40719

Float

Read/Write

-

ACTION21.SOURCEPARAM

40720

Float

Read/Write

-

ACTION22.SOURCEPARAM

40721

Float

Read/Write

-

ACTION23.SOURCEPARAM

40722

Float

Read/Write

-

ACTION24.SOURCEPARAM

40723

Float

Read/Write

-

ACTION25.SOURCEPARAM

40724

Float

Read/Write

-

ACTION26.SOURCEPARAM

40725

Float

Read/Write

-

ACTION27.SOURCEPARAM

40726

Float

Read/Write

-

ACTION28.SOURCEPARAM

40727

Float

Read/Write

-

ACTION29.SOURCEPARAM

40728

Float

Read/Write

-

ACTION30.SOURCEPARAM

40729

Float

Read/Write

-

ACTION31.SOURCEPARAM

40730

Float

Read/Write

-

ACTION32.SOURCEPARAM

40731

Float

Read/Write

-

Related Topics

Action Table